Embedded Software
Camera Enablement Package for NVIDIA®’s Jetson boards
Version: 1.0.0
Operating System: Linux ARM
To run a Basler Add-on Camera Kit with an NVIDIA Developer Board of the Jetson family, you need a suitable JetPack / Linux for Tegra (L4T) version.
This CEP is a compressed file and contains release notes that list the supported L4T versions, and a readme document that contains a description of the installation and lists compatible boards. It contains the following components:
- the Basler camera kernel driver
- device-tree overlays for supported boards
- GenTL Producer
- the pylon Viewer application
In this way, you can use a Basler dart BCON for MIPI camera with an NVIDIA Developer Board from the Jetson family.