There are two installation packages. If you are going to perform the installation on Ubuntu 18.04 or above, use the Basler_blaze_SDK-4.0.0.6-efd9603a-Linux_x86_64.tar.gz archive. Otherwise, use the Basler_blaze_SDK-4.0.0.6-efd9603a-Linux_x86_64_no_viewer.tar.gz archive. The SDK in the "no_viewer" archive is supported for Ubuntu 16.04 or above, but doesn't include the blaze Viewer tool. The "no_viewer" SDK may run on several other Linux distributions if they provide libstdc++6.0.21 or above.