*WARNING*: To update the camera's firmware to firmware version 4.0 or above, the camera's current firmware version has to be at least 2.3.0. If the current firmware version is below 2.3.0, you first have to update the camera to firmware version 3.0.1. Afterwards, you can perform an update with firmware version 4.0.1. Firmware update packages and update instructions can be downloaded here: https://www.baslerweb.com/baslermedia/blaze-getting-started/?dir=Firmware *Note*: To operate blaze-101 cameras with firmware version 4.0.0 or above, the Basler blaze SDK 3.0.0 or above is required. For using new features introduced by firmware versions 4.0, you have to update to Basler blaze SDK 4.0 or above. The latest Basler blaze SDK can be downloaded here: https://www.baslerweb.com/baslermedia/blaze-getting-started/?dir=SDK